Dear Team,
According to the image attached i have some doubts regarding Regenerative braking.
1) Please correct me if i am wrong that the Regenerative braking will only occur when there is no input voltage or current is given (under free run) to the motor and motor is providing the current, So why there is concept of providing negative Iq ref value? please elaborate.
2) In regenerative braking the motor should act as a battery charger that provides constant voltage(irrespective of current value) because battery lines are directly connected to the controller. So How it can be done?
3) According to me if i accelerate the motor by potentiometer and suddenly make the pot readings to zero then the motor running will generate the regenerative current. So How i can monitor that value and use that value feed back to battery?
Thanks.