Other Parts Discussed in Thread: TMS320F28377S, AMC1304M05
Hi Folks,
This is my first post to E2E. I found it very helpful to learn things quickly and I appreciate this effort from TI.
I am a beginner in Microcontrollers and I am using Delfino LaunchPad in my master internship. I have a querry from SDFM module of TMS320F28377S.
a) Why the Data Rate of Sigma Delta Modulator (ADC) depends on the input control unit of digital filter (SDFM) ? I mean, if I am operating in Mode_0 and my modulator clock is 20MHz, my modulator data rate will also be 20MHz?
If I use sinc3 filter with maximum OSR 256 at a clock frequency of 20Mhz, I get filter Data Rate of 78KSPS but my filter Latency is three times more than time period of my sinc3 filter ( which should be 1 / Filter Data rate = 1/ 78KSPS = 12.9 micro-seconds) i-e 38.7 micro-seconds
b) So my confusion is, if the output of filter could be seen on oscilloscope for example or in software, what would be sinc3 filter waveform frequency? 1/ Latency or 78 KSPS? Because their reciprocals aren't equal.
I would be thankful if someone can clear my confusion.
Best Regards,
Andreas