I'm not sure if adding a post to an already answered question gets anyone's attention or not, so I'm reposting here. Sorry for the clutter, but here goes:
"../2837x_RAM_lnk_cpu1.cmd", line 65: error #10099-D: program will not fit into available memory. run placement with alignment/blocking fails for section ".ebss" size 0x1b29 page 0. Available memory ranges:
RAMGS3 size: 0x1000 unused: 0x847 max hole: 0x802
RAMGS4 size: 0x1000 unused: 0x1000 max hole: 0x1000
RAMGS5 size: 0x1000 unused: 0x1000 max hole: 0x1000
error #10010: errors encountered during linking; "Trireme.out" not built
gmake: *** [Trireme.out] Error 1
Here is the linker entry
.ebss : >>RAMGS3 | RAMGS4 | RAMGS5, PAGE = 0
As you can see, the combined size is 0x3000, but the linker refuses to use it all.