Other Parts Discussed in Thread: DRV8312
1: Which lab do I need to use to identify my motor? (Lab 2a or Lab 2c)
I use DRV8312-C2 and F2805x controlCard
Here are my motor's name and parameters: FAULHABER BLDC Series 1628024B
Terminal inductance, phase to phase L: 525uH
No-load current: 0.052A
Max current: 0.41A
I used both lab 2a and 2c to identify my motor, but the values come out differently, which one do I need to choose?
Do I still need to make changes on USER_MOTOR_FLUX_EST_FREQ_Hz (20 to 100) and USER_PWM_FREQ_kHz (45.0 to 60) if I use Lab2a? Or only make these changes on Lab2c?
2: How do I set my USER_MOTOR_RES_EST_CURRENT and USER_MOTOR_IND_EST_CURRENT?
Is base on 10-20% of maximum current or No-load current?
3. What cause my gMotorVars.Lsd_H and gMotorVars.Lsq_H equal to 4.98136199e-10 or 3.1138512e-11?
Thank you for the help!!!