This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLA1mathTables not found.

Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28069

Hi all

I am using TMX320F28075 device.

I want to use CLA for the same device.

I linker command file i am using is 

C:\ti\controlSUITE\device_support\F2807x\v210\F2807x_common\cmd\2807x_FLASH_CLA_lnk_cpu1.cmd

But i am not able to find the declaration of "CLA1mathTables".

due to that i am getting a warning of 

"Description Resource Path Location Type
#10247-D creating output section "CLA1mathTables" without a SECTIONS specification test C/C++ Problem"



looking in the details

I have seen in demo application of CLA that is given at

C:\ti\controlSUITE\libs\math\CLAmath\v4_02_00_00\examples\2806x_cos

they have used the command file which has "CLA1mathTables"



what should i do resolve the warning?