As per the reference guide www.ti.com/.../sprufb0d.pdf the procedure to change the PLL Control Register has the following steps:
1. Check if PLLSTS[MCLKSTS] is not equal to 1
2. Set PLLSTS[DIVSEL] to 0
3. Set PLLSTS[MCLKOFF] to 1
4. Set new PLLCR value
5. Wait for PLL to lock.
1. What are the implications if we skip steps 1, 2 and 3 in the above described procedure under normal condition (non-limp mode)?
2. What are the implications if we skip steps 1, 2 and 3 in the above described procedure under limp mode?