This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Jiri Panacek85 in C2000™ Microcontrollers F2802x Peripheral Driver Library - bug in ADC_setVoltRefSrc(...) ?

Other Parts Discussed in Thread: CONTROLSUITE

Hi, 

it's me again :) . I think there is another bug in the F2802x Peripheral library. The function

ADC_setVoltRefSrc(myAdc, ADC_VoltageRefSrc_Ext); 

does not set external voltage reference. It should set bit 3 (ADCREFSEL) in ADCCTL1 register but it sets bit 0 instead. Could you please check and eventually add it to the bug list ?

Library : C:\ti\controlSUITE\device_support\f2802x0\v230\

Best regards, 

Jiri