Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hi chris and all,
i want to use an external current sensor (HASS s-300).
It has input of 5V and sensitivity is 2.083 mV/A and range is +/-900A. How can i scale down its output e.g. (0V to 5V) to (0V to 3.3V)? should i have to apply voltage divider?
Also I want to use this with DRV8301 board by eliminating Ia,Ib,Ic wires connection of DRV8301 with Instaspin and placing 3 wires of HASS s-300 sensor.
To use this should i have to only make change in USER_ADC_FULL_SCALE_CURRENT (1800);? and USER_IQ_FULL_SCALE_CURRENT (900);
Thanks.