This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uploading program failure F28377S

Hi

I am trying to upload a new program with XDS100v2 to a new  F28377S chip , and i am getting the next warnning :

C28xx_CPU1: Error occurred during flash operation: Timed out waiting for target to halt while executing wr_pll.alg
C28xx_CPU1: Error writing the PLL values (Flash algorithm timed out). Operation cancelled.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\Users\MARK\workspace_v6_1\TOPI_MC\F2837x_FLASH\TOPI_MC.out: Load failed.

until now we had no problems like this one .

my BOOT-MODE pins GPIO72/GPIO84 are both set to 1.

if for example i am trying to upload a program running from RAM , it successfuly upload it , but its accting strange and i dont see the variables changes in the  expression box.

also i tried to set the  GPIO72/GPIO84 to 1/0 for wait mode , this helps and it flashes the program , but still the its seems not working as the variables dosent change in the  expression box.

also the power consumption is very low.

whould be happy to some advisement

best regards

MARK