Other Parts Discussed in Thread: CONTROLSUITE, MOTORWARE, LAUNCHXL-F28069M
Setup
- Running everything on Linux (Ubuntu 16.04)
- Running controlSUITE and MotorWare using Wine.
- Connected to LAUNCHXL-F28069M
- CCS 6.2
Problem
I am trying to do the Project labs that come with the MotorWare (1.00.17) and during compiling I got an error.
No recipe for F28069_ram_link.cmd needed for proj_lab01.out
I opened the said file but it was empty (or not opening) so I removed it from the project. But now when I trying to debug, I get the following error.
C28xx: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
Please help in resolving this.