Other Parts Discussed in Thread: CONTROLSUITE, MOTORWARE
Hello together -
I want to use the InstaSPIN-solution with a custom designed board.
The power-FETs and drivers are very fast and tests showed me so far, that operating at a
PWM-frequency of 350kHz is no problem for the power-bridge.
I have spent much time until now studying the behavior and the characteristics of Instaspin and found that there seems to be a upper limit
around 90kHz for the USER_PWM_FREQ in the labs.
So my question:
What can i do to operate Motor-Identification and Motor drive with InstaSPIN at a freqeuncy of 350kHz ?
What do i have to change in software and what are the correct parameters ?
I hope you can help me by providing some tips or reference.
Andreas