Other Parts Discussed in Thread: DRV8301
Hi all,
I am reading ADC values of phase current sensors in DRV8301.
I did the following for that i made a function in hal.h
static inline CurrentSensorRead_A(HAL_Handle handle)
{
HAL_Obj *obj = (HAL_Obj *)handle;
int gIAread = 0;
gIAread = ADC_readResult(obj->adcHandle,ADC_ResultNumber_1);
return gIAread;
}
and i call that function inside while loop in project man function.
Is there a mistake i am doing? as in watch window the ADC values are fluctuating (say in between 2061-2072).
Thanks.