Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28377S
Hi sir/madam
I have run into problems when connecting F28377S and the CCS. Here is the steps that I have done:
- I installed CCS 6.2 and control suite.
- F28377S is connected to PC with USB cable
- I took the example file from C:\ti\controlSUITE\device_support\F2837xS\v210\F2837xS_examples_Cpu1 to test the QEP with the encorder and launched debug
- It asked me to create a NewTargetConfiguration file and to choose the connection and device
- First I chose the Spectrum Digital C2000 XDS510LC Emulator and couldn't found the correct board number (TMS320F28377S). When I searched for any helpful imformation and realized that it is the wrong emulator i had chosen.
- Then I chose the Spectrum Digital XDS510USB Emulator and found the TMS320F28377S.
- When I tested the connection after saved, there was a error pop up like below:
[Start: Spectrum Digital XDS510USB Emulator_0]
Execute the command:
%ccs_base%/emulation/drivers/sdjtag.exe -f %boarddatafile% -v -X reset -X scantest
[Result]
** BoardFilePath: C:\Users\Jack-2\AppData\Local\TEXASI~1\CCS\ti\0\0\BrdDat\testBoard.dat
** Resetting Emulator
ERROR -- XDS510-USB Emulator not connected/enumerated[End: Spectrum Digital XDS510USB Emulator_0]
[Start: UARTConnection_0]
Execute the command:
The Diagnostic Command is not defined in the connection properties.

Is there anything I have doing it wrong ?
With regards,