This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28379D datasheet question

Hi Champs,

My customer asked about Reset Lo(RLS1) max/min time. in datasheet, it showed only typ time. Do we have RLS1 max/min time ? 

For ADC 12-bit single-ended mode, our SPEC based on VREFHI=2.5v. Do we have ENOB SPEC base on VERFHI=3,3v ? 

thanks for your reply in advance.

  • Hi Lisa,

    For ADC ENOB, 2.5V VREFHI is worst case.  Increasing the VREFHI voltage gives a larger range for the internal ADC noise to spread out over, so you would see a very slight improvement in SNR of maybe 1dB.  

    Do be cautious, however, because VREFHI < VDDA is a hard requirement; ADC performance will be negatively impacted if VREFHI = 3.3V and VDDA = 3.3V and VDDA starts to drift lower than 3.3V.  For this reason, we recommend a 3.0V reference instead.  Alternately, you could use a configurable regulator for VDDA and VDDIO to set these rails a couple percent higher than 3.3V. 

  • Hi Devin,
    I see. Thanks for reply. Do we have data for Reset Lo(RLS1) max/min time ? thank you!