Other Parts Discussed in Thread: MOTORWARE, DRV8301
We are successfully using your DRV8301-69M-Kit (D) and LAUNCHXL Board together with motorware 1.01.00.16.
For analysis purpose we need to show customer current values for our 12 V, 2.4 A BLDC Motor.
We calculated the effective phase current values by RMS calculation over one electrical rotation for the three AdcData.I.values. Calculated values are sufficiently matching measured values at different load situations.
But the Motor current sum calculation is quite inaccurate. We used Iq and AdcData.U.values (U also as RMS over one rotation) and your answers to the "F28027 + DRV8301 motor power measurement" question. But their accuracy is not very good. Can you give a hint how to calculate the total motor current with motorware?
Thanks in advance for your support!