Hi,
I'm new in PLC systems.
I have a TI TMDSPLCKIT-V3. My idea is to develop CCS program using example project. I download 'Flex OFDM Development Package V1300'. There is an error when i try to flash firmware with the example code in 'Flex OFDM Development Package V1300'. The software was written based on the microcontroller F28335. However, the microcontroller hardware of TMDSPLCKIT-V3 is F28069.
I'd like someone tell me how to develop OFDM project with TMDSPLCKIT-V3 (F28069+AFE031). It's highly appreciate if someone could offer me a Flex OFDM software link for F28069?
Thanks for your help.