I have a Transphorm PV Inverter 1 phase bridge eval board (TDPV1000E0C1) and would like to make some modifications to the output wave shape. It looks like the shape of the output wave is defined in the array wSinTab in the SolarHv_DCAC-main.c file starting at line 374. Can these values be changed to shape the output wave to something other than a sine wave?
I'll also need to change the output wave frequency. Would this be done in the GEN_SIN_COS block by changing the dwPll_Trace_Freq value?
Thanks!