Other Parts Discussed in Thread: MOTORWARE
Hi Chris and all,
We are using motorware lab5a with resolver feedback. We have connected the inverter to a 330V battery pack. Once we apply a higher Iq_ref command (ex: 600A) with the load motor accelerate fast without any issue. But when we apply a zero Iq_ref (0A) command form higher Iq_ref command (600A)while the motor is rotating with the load, motor brake with oscillations. It feels like pulse braking. a very high voltage (500V) appears on the dc bus during this kind of braking event. After few oscillations it becomes normal deceleration. This did not occur in low Iq_ref command (ex:200A).
1) Is this normally expected?
2) If it is normal, What is the theory behind that?
3) How we could avoid this pulse braking?
4) Can we apply Zero Iq_ref command suddenly after high Iq_ref command (ex : 600A) with load condition.
Thank you.