Hi,
I'm using DRV8312 and F2805x. The default setting:
USER_IQ_FULL_SCALE_CURRENT_A (10 ) A
AND USER_ADC_FULL_SCALE_CURRENT_A (17.30) A
I am not able to achieve my motor spec from above setting. (not enough current for high acceleration or torque)
Basically, my motor is not able to run at its full performance under this current scaling.
So I modified the Current scaling as following, I am able to draw more current into my motor under same motor parameter setting at user.h
USER_IQ_FULL_SCALE_CURRENT_A (5) A
AND USER_ADC_FULL_SCALE_CURRENT_A (8.65) A
BUT it still not able to produce as much torque as it should be. only 1/4 of my max torque(12mNm)
The max current for my motor is 0.41A. Is there any document can help me to set this scaling correctly to max out my motor's performance?