Other Parts Discussed in Thread: LAUNCHXL-F28379D, CONTROLSUITE, TMDSDOCK28379D, TMDSCNCD28379D
We would like to buy some LAUNCHXL-F28379D boards:
www.ti.com/.../LAUNCHXL-F28379D
And we want to have the access to all the GPIO channels. We would like to know if LAUNCHXL-F28379D itself can provide us with the access to all the GPIO channels or we need to buy a corresponding BoosterPack for LAUNCHXL-F28379D?
In the "User's Guide" of LAUNCHXL-F28379D (http://www.ti.com/lit/ug/sprui77/sprui77.pdf), it is said that:
"Connecting a BoosterPack The F2837xD LaunchPad is the perfect experimenter board to start hardware development with the F2837xD devices. All of the connectors are aligned in a 0.1-in (2.54-mm) grid to allow easy and inexpensive development of add on boards called BoosterPacks. These satellite boards can access all of the GPIO and analog signals."
It seems that we need an additional BoosterPack to get the access to all the GPIOs. If this is really the case, then can anyone provide us with the product code of the BoosterPack?
Thanks!