This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLA Watchdog Reset vs Emulator Reset

I'm trying to use the CLA on a F28069 and F28377D.  My application resets via the watchdog under certain conditions to restart the application if something has gone wrong.  Prior to using CLA, this reset/restart worked.

After adding the CLA, the watchdog reset/restart no longer works.  My application gets stuck waiting for a CLA interrupt to the CPU to indicate that a CLA task (started via IACK) has completed running.  However, if I CPU Reset/Restart from CCS, the application restarts fine as the CLA interrupt to the CPU is received.

What differences are there between a watchdog reset and emulator reset with regards to the CLA that could cause the CLA to not respond when watchdog reset but respond when emulator reset?

Note: I did see this post:   Unfortunately, it does not seem to solve the issue for me.  I've already added the memcpy from flash to RAM to support the application running from flash, yet the CLA does not respond after a watchdog reset.

Thanks,
Joseph

  • Hi Joseph,

    Please check if you are enabling the CLA clock in your application (via PCLKCRx register). On emulation reset, this is taken care by Gel file which will not happen incase of WD reset unless application code does it.

    Regards,
    Vivek Singh
  • Hi Vivek,

    Thanks for the suggestion.  My application code for setting up the CLA does enable the CLA clock after the memcpy() for CLA code and prior to writing any CLA registers in the Delfino by:

        SysCtlPeripheralEnable((uint32_t) SYSCTL_PERIPH_CLA1);

    and in the Piccolo by:

        SysCtrlRegs.PCLKCR3.bit.CLA1ENCLK = 1;

    Also, I have checked the MVECT values in the Expressions window, which show they have been programmed to the correct address/offset.  I believe the MVECT registers cannot be written unless the CLA clock is enabled.

    Any other ideas?

    Best Regards,

    Joseph

  • Joseph,

    After the watchdog reset are you reconfiguring the CLA registers?
  • Hi Vishal,

    Yes, the CLA configuration is run after watchdog reset.

    Best Regards,
    Joseph
  • Hmm, i wonder if its the same issue as in this post: e2e.ti.com/.../386841

    Essentially when the JTAG is connected and you do a reset you go through a different path through the boot rom (EMU mode) versus a watchdog reset in standalone mode (boot to flash). So in standalone mode you have to make sure the code is copied from flash to ram, the constants (.cla_const) is also copied.

    You mentioned the code is stuck in the while loop, that is why i asked if the CLA registers were being configured after a WD reset. Since they are im assuming the CLA code is not at its intended location (RAM) and so the CLA starts fetching garbage opcode and basically stalls, which is why the c28x is still idling in the while loop.

    I go over some of these things with the original poster in the above link.
  • Hi Vishal,

    Thanks for the suggestions.  I have read that thread that you linked, but I went over it again more carefully per your suggestion.

    1) I believe I am copying the CLA program. Excerpts from my linker .cmd:

    Hi Vishal,
    
    I have read that post, but I went over it again more carefully per your suggestion.
    
    1) I believe I have to be copying the CLA program as the linker file specifies loading it into flash and there is no other way for the CLA program to be in RAM after loading from the emulator other than the memcpy() shown below.  Excerpts from my linker .cmd:
    
    MEMORY
    {
    PAGE 0 :   /* Program Memory */
        L3DPSARAM   : origin = 0x009000, length = 0x001000     /* L3   DPSARAM, CSM secure, CLA Program RAM, within SP range */
        OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
        #ifdef FLASH_BOOT
        // restrict from full length of 0x1FF80 to sector A/B/C/D/E length of 0x13F80
        FLASH       : origin = 0x3E4000, length = 0x013F80     /* on-chip FLASH */
        #else
        // restrict from full length of 0x1FF80 to sector A/B/C length of 0xBF80
        FLASH       : origin = 0x3EC000, length = 0x00BF80     /* on-chip FLASH */
        #endif
        Cla1Prog                : LOAD = FLASH
                                  RUN  = L3DPSARAM                                            /* Link to CLA Program RAM */
                                  LOAD_START(_cla1prog_load_start),
                                  LOAD_SIZE(_cla1prog_load_size),
                                  RUN_START(_cla1prog_run_start),
                                  PAGE = 0, ALIGN(4)
    

    And from the CLA initialization function prior to writing to enablging the clock to the CLA and writing to the MemCfgRegs and Cla1Regs:

        (void) memcpy(&cla1prog_run_start, &cla1prog_load_start,
            (int16_t) &cla1prog_load_size);

    2) Elliott (original poster of above link) had an issue on power up which I don't think applies since my case does not involve power cycling.  Power should be  stable unless the watchdog reset somehow causes the voltage to droop.

    3) You mentioned copying .cla_const which I was not doing, but I believe invalid constants in my application only causes an invalid PWM value to be written by the CLA, but should not prevent the CLA from running.  To rule it out, I went ahead and tried copying from flash with the following addition to the linker .cmd:

    PAGE 1 :   /* Data Memory */
    
        M01SARAM    : origin = 0x000000, length = 0x000800     /* on-chip RAM block M0, M1, within SP range */
        PIEVECT     : origin = 0x000D00, length = 0x000100     /* peripheral interrupt expansion */
        CLA2CPU     : origin = 0x001480, length = 0x000080     /* Part of PF0 - CLA to CPU Message RAM */
        CPU2CLA     : origin = 0x001500, length = 0x000080     /* Part of PF0 - CPU to CLA Message RAM */
        L01DPSARAM  : origin = 0x008000, length = 0x000C00     /* L0-1 DPSARAM, CSM secure, within SP range */
        L2DPSARAM   : origin = 0x008C00, length = 0x000400     /* L2 DPSARAM, CSM secure, within SP range */
        .const_cla              : LOAD = FLASH                                       PAGE = 0
                                  RUN  = L2DPSARAM                                   PAGE = 1 /* Link to CLA Program RAM */
                                  LOAD_START(_cla1const_load_start),
                                  LOAD_SIZE(_cla1const_load_size),
                                  RUN_START(_cla1const_run_start),
                                  ALIGN(4)
    

    And the following in the CLA initialization:

        (void) memcpy(&cla1prog_run_start, &cla1prog_load_start,
            (int16_t) &cla1prog_load_size);
        (void) memcpy(&cla1const_run_start, &cla1const_load_start,
            (int16_t) &cla1const_load_size);

    I think those were the only 3 issues suggested from the above link and your reply above, however I don't think any of them are causing the CLA non-responsiveness after watchdog reset in this case.  Any other ideas on what is different between emulator and watchdog reset that could cause this?

    Best Regards,

    Joseph

  • There shouldn't be much difference between the resets except for the route through the boot code; at least to my knowledge that is the only difference. After a watchdog reset and the IACK instruction do you see the MIRUN bit for that task get set? Can you connect to the CLA and see where the execution is at  - even if you dont connect to the CLA you can inspect the Cla1Regs.MPC to see if it changes - that would mean the CLA is executing some code.

  • I hope this issue is resolved?
  • Vishal_Coelho said:

    There shouldn't be much difference between the resets except for the route through the boot code; at least to my knowledge that is the only difference. After a watchdog reset and the IACK instruction do you see the MIRUN bit for that task get set? Can you connect to the CLA and see where the execution is at  - even if you dont connect to the CLA you can inspect the Cla1Regs.MPC to see if it changes - that would mean the CLA is executing some code.

    Hi Vishal,
    Sorry for the delayed reply as I did not have a system to test this on for a while.  I put the MIRRUN bits and MPC registers in the Expressions window with auto-refresh and a breakpoint where I issue IACK and the watchdog reset.  After a CPU Reset and Restart, I see some of the MIRUN bits go to 1 and the MPC changes value.  I see the code break at the watchdog reset and after reset, I see tha it breaks at IACK, but then I do not see the MIRUN bits go to 1 or the MPC change. 
    I just noticed that IACKE is successfully set after the CPU Reset and Restart, but after a watchdog reset my application tries to set to enable IACK, but it is not set after the write.  I don't see anything in the TRM that suggests that it is possible for a write to MCTL.IACKE to not succeed, so this seems like unexpected behavior.

    Vivek Singh said:
    I hope this issue is resolved?

    Hi Vivek,
    Unfortunately, it has not yet been resolved.  I'm not sure what 
    Best Regards,
    Joseph
  • I found the problem. I was missing EALLOW prior to setting SysCtrlRegs.PCLKCR3.bit.CLA1ENCLK. What threw me off is that this would work after a CPU Reset/Restart from a debugger which it should not. Presumably, there was magic timing after a CPU Reset/Restart from the debugger where EALLOW was enabled elsewhere that would allow it to succeed in this special case, though normally it should fail as it did after a watchdog reset.

    Regards,
    Joseph