This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C: F28M35x Flash Programming

Part Number: F28M35H52C
Other Parts Discussed in Thread: UNIFLASH

Hi,

We are using CSS and UniFlash to program both M3 and C28 over XDS100v2.

1. Is there any other tools for F28M35x Flash Programming?

2. Is there any tools to communicate with F28M35x over JTAG pins directly (without XDS100v2)?

Thanks,

T.

  • Hi,

    1. Is there any other tools for F28M35x Flash Programming?

    Yes, there are other 3rd party tools like "C2000 Gang Programmer" can be used for flash programming.

    2. Is there any tools to communicate with F28M35x over JTAG pins directly (without XDS100v2)?

    Could you elaborate a bit more on this. XDS100v2 is emulator and there are many other emulators which can be used (e.g. SD XDS510USB, BH XDS560 etc). CCS is tool which provide GUI interface (IDE) to connect to device via these emulators (JTAG pins). Apart from CCS we do not have any other GUI interface.

    Regards,

    Vivek Singh

     

  • Thank you for C2000Gang Programmer info.

    1. Can we connect this C2000 Gang Programmer to H52C1 Board? Though DIMM100 connector ?
    2. Do we have any solution for upgrade firmware on both M3 and C28 in the field?
    Using some BootLoader over Ethernet?

    Thanks,
    Tim
  • Hi,

    You can use C2000-GANG Programmer (see TI website). The mentioned MCU can be programmed via JTAG directly from programmer.

    Let me know if you have any questions.

    Best regards,

    Gregory Czajkowski
    Elprotronic Inc.