Part Number: TMS320F28377D
Other Parts Discussed in Thread: CONTROLSUITE
In the flash programming examples, it shows setup, erase and write of several sectors. Consider the following two TI example code excerpts from \ti\controlSUITE\device_support\F2837xD\v210\F2837xD_examples_Dual\flash_programming\cpu01:
1)
//
// Erase Sector B
//
oReturnCheck = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector,
(uint32 *)Bzero_SectorB_start);
//
// Wait until FSM is done with erase sector operation
//
while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}
//
// Verify that SectorB is erased. The Erase step itself does a verify as
// it goes. This verify is a 2nd verification that can be done.
//
oReturnCheck = Fapi_doBlankCheck((uint32 *)Bzero_SectorB_start,
Bzero_16KSector_u32length,
&oFlashStatusWord);
2)
// Example: Program 0xFF bytes in Flash Sector B with out ECC
// Disable ECC so that error is not generated when reading Flash contents
// without ECC
//
Flash0EccRegs.ECC_ENABLE.bit.ENABLE = 0x0;
for(i=0, u32Index = Bzero_SectorB_start;
(u32Index < (Bzero_SectorB_start + WORDS_IN_FLASH_BUFFER)) &&
(oReturnCheck == Fapi_Status_Success); i+= 8, u32Index+= 8)
{
oReturnCheck = Fapi_issueProgrammingCommand((uint32 *)u32Index,
Buffer+i,
8,
0,
0,
Fapi_DataOnly);
while(Fapi_checkFsmForReady() == Fapi_Status_FsmBusy);
if(oReturnCheck != Fapi_Status_Success)
{
//
// Check Flash API documentation for possible errors
//
Example_Error(oReturnCheck);
}
//
// Read FMSTAT register contents to know the status of FSM
// after program command for any debug
//
oFlashStatus = Fapi_getFsmStatus();
//
// Verify the values programmed. The Program step itself does a verify
// as it goes. This verify is a 2nd verification that can be done.
//
oReturnCheck = Fapi_doVerify((uint32 *)u32Index,
4, Buffer32+(i/2),
&oFlashStatusWord);
if(oReturnCheck != Fapi_Status_Success)
{
//
// Check Flash API documentation for possible errors
//
Example_Error(oReturnCheck);
}
}
Two comments concern me:
1) "The Erase step itself does a verify as it goes. This verify is a 2nd verification that can be done".
2) "The Program step itself does a verify as it goes. This verify is a 2nd verification that can be done."
Is there any value/added confidence in calling Fapi_doBlankCheck(...) or Fapi_doVerify(...)? If so, can you clarify what?
Thanks!
Stephen