Other Parts Discussed in Thread: MOTORWARE
I want to be able to control two motor at the same time from one TI processor. So, I started looking at Lab 6e, Lab 10d,
Lab 6e - Dual Motor Sensorless - It says Sensorless, , I was expecting it to be similar to Lab 4, Lab 4a, Lab 5a, but for 2 motors. is it just current / torque control lab ? But I dont see a way to tune the PI gains for the current controller. Please help. There is also no writeup, directions for the Lab 6e, just the code which is a very different in architecture compared to rest of Motorware labs. So, this will need me to understand and locate every variable again from scratch. Even if i use spintac controllers , the current controller used to be just a PI controller and so the first thing i had to do was tune that before moving ahead with spintac velocity or position controllers. So, I am trying to do the same first with Dual Motors.
Lab 10d - Dual Motor Sensorless Velocity Control. Is this similar to Lab 5d, lab5e? but for 2 motors
Lab 11d - Dual Motor Sensorless Velocity Control. - how is it different compared to Lab 10d? both labs have the same names.
Lab 12c : Dual Motor Sensored Velocity Control. Is it similar to Lab 12b, but for 2 motors.
Lab 13f : Dual Motor Sensored Position Control . Is this similar to Lab 13b ? but for 2 motors