Part Number: F28M35H52C
Hi TI,
We are planning to use F28M35H52C1RFPT part from TI. We have small doubts in CAN interface. I have used PE6_GPIO30 (22 nd pin) is RXD , PE7_GPIO31 (23rd pin) is TXD and PJ7_GPIO63(97th pin) is clock for CAN peripheral from the DSP . 10MHz oscillator is connected to PJ7_GPIO63(97th pin) to source the CAN interface clock. As per datasheet recommendation PJ7_GPIO63(97th pin) XCLKIN in is upto 60MHz.
Shall i proceed with 10MHz external oscillator or reduce the frequency ?
Please guide me
Regards,
Rajkumar