This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2806: Motorware17

Part Number: TMS320F2806
Other Parts Discussed in Thread: MOTORWARE

In motorware 17, the EST_getAngle_pu function is documented that the return value will be between _IQ(0.0) and _IQ(1.0), which is true in Forward but in the Reverse direction, the value returned is between _IQ(0.0) and _IQ(-1.0).  I found the thread below which described the same issue back in 2014.  Has anything been done about this or is there a workaround?

Regards,

Sandy Moore

In Motorware_13, the EST_getAngle_pu function documentation mentions a return value between _IQ_ 0.0 and 1.0, but when running a reverse direction / negative speed, the actual value is between zero and MINUS_1.

....

Regards,

Harry Kroonen

3 Replies