A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am currently trying the i2c_eeprom example code in CCS. In the example there only 2 bytes data send that are 0x12, 0x34. When I just send 2 byte data and try to read it back, it was success.
In the message buffer there has some explanation that the maximum data can send is 14, but when I trying to send 14 data from master, I have problem to read the data, I just can read 2 data that is first byte & second byte. Do you know how to read the 3rd to 14th data?