Other Parts Discussed in Thread: TMS320F28379D, LAUNCHXL-F28379D, CONTROLSUITE
Hello,
I am new to the TMS320F28379D microcontroller and I have an issue with programming this microcontroller. I am using the launch pad LAUNCHXL-F28379D and following examples provided by TI, I have managed to program the TMS320F28379D to output a PWM output and then sample it back with the ADC while blinking an LED on the Launch Pad. The program is working fine when I build and load the program in Debug mode using Code Composer. My issue is that the code works only when I have Code Composer in debug mode. If I disconnect the launch pad from my PC and reconnect the program in the controller does not restart. I have to re-open Code Composer, build again and load through Debug mode. I do not know if it is an issue of booting to RAM instead of Flash, since at this point I have not really understood the whole booting process on this controller.
Any help would be greatly appreciated.
Thanks
Dan