This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ACI Scalar Control in Low Speeds

Hi Everyone,

I have a question related with Encoder speed measurement. I have a quadrature encoder in my system and I read the speed successfully. But there are only 60 teeth on motor side. Therefore I have little problem while reading low speeds and this problem affect my motor control at low speeds.

I am using f28377d in my control card and I am trying to control Induction Machine with v/f control. Does anyone have any suggestion to improve the control at low speeds?

To read the low speeds successfully,  I tried to make register change in my control loop i.e. I set the QCAPCTL.UPPS register to 2 at start , and then change it to 4 when it goes over 120rpm. But in c2000 forum it is said that it is a bad idea that change the register dynamically. 

Any comment would be appreciated.

Thank You