Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH,
I am trying to use a Spectrum Digital XDS200 USB on Windows 10 64-bit with UniFlash and I get the following error:
Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.504.1)
Not sure if this is a driver issue. The XDS200 shows up in Windows as a USB Composite device in device manager (generic name). I would expect a non generic name if it enumerated properly and the correct drivers were installed. I've tried installing CCSv7 to see if the drivers are available there. No luck.uninstalled and re-installed UniFlash. Still no luck. The left Green LED is lit. I've plugged it into two different USB ports and still get the same issue.