Part Number: TMS320F28027F
Hi,
We are helping an aquarium pump customer to migrate their pump controller platform from trapezoidal drive (Sensorless BLDC, control by percentage of PWM duty) to InstaSPIN solution, one of the characteristics of this application is the load of the system are different for each end customer as they install the aquarium pump and pipes system differently. This leads to, the max. power and max. rpm of the pump in each pump system will be different.
The current solution of sensorless trapezoidal is straight forward to control, just adjust the PWM duty, the pump can be set to max. required performance (that according to the pump system loading) just by setting PWM to 100% duty.
However, when migrating to InstaSPIN solution, which runtime parameters should be used, which is analogy to setting the duty of PWM ?
Thanks in advance.
Regards,
Nikolaus