Hello Folks,
i have the SPI running on a TMS320F28377S and have a time jitter between CLK ans MOSI.
I have configured the SPI to put out 12 bits per character, and for a test i use a bit coded value of 0b110010101100.
On the scope i see the last bits are missing, while the clock starts to early.
Is there something i haven´t considered in the initialisation?
Below see the scope´s screenshot and my SPI_Init and ISR.
best regards!
#define SPI_BRR ((200E6 / 4) / 500E3) - 1
void DACSink::Init()
{
EALLOW;
//ClkCfgRegs.LOSPCP.bit.LSPCLKDIV = 0;
//SpiaRegs.SPICCR.bit.HS_MODE = 0x1;
//
// Enable internal pull-up for the selected pins
//
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
//GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0; // Enable pull-up on GPIO16 (SPISIMOA)
//GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0; // Enable pull-up on GPIO18 (SPICLKA)
GpioCtrlRegs.GPBPUD.bit.GPIO58 = 0; // Enable pull-up on GPIO16 (SPISIMOA)
GpioCtrlRegs.GPBPUD.bit.GPIO60 = 0; // Enable pull-up on GPIO18 (SPICLKA)
//
// Set qualification for selected pins to asynch only
//
// This will select asynch (no qualification) for the selected pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPBQSEL2.bit.GPIO58 = 3; // Asynch input GPIO16 (SPISIMOA)
GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3; // Asynch input GPIO18 (SPICLKA)
//
//Configure SPI-A pins using GPIO regs
//
// This specifies which of the possible GPIO pins will be SPI functional
// pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPBGMUX2.bit.GPIO58 = 3; // Configure GPIO16 as SPISIMOA
GpioCtrlRegs.GPBGMUX2.bit.GPIO60 = 3; // Configure GPIO18 as SPICLKA
GpioCtrlRegs.GPBMUX2.bit.GPIO58 = 3; // Configure GPIO16 as SPISIMOA
GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 3; // Configure GPIO18 as SPICLKA
//
// Initialize SPI FIFO registers
//
SpiaRegs.SPIFFTX.bit.TXFFINTCLR = 1;
SpiaRegs.SPIFFTX.bit.SPIFFENA = 1;
SpiaRegs.SPIFFTX.bit.TXFIFO = 0; //reset fifo pointer
SpiaRegs.SPIFFTX.bit.TXFIFO = 1;
SpiaRegs.SPIFFTX.bit.TXFFIENA = 1;
SpiaRegs.SPIFFTX.bit.TXFFIL = 0;
SpiaRegs.SPIFFTX.bit.TXFIFO=1;
SpiaRegs.SPIFFRX.bit.RXFIFORESET=1;
// Initialize SPI-A
// Set reset low before configuration changes
// Clock polarity (0 == rising, 1 == falling)
// 16-bit character
// Enable loop-back
SpiaRegs.SPICCR.bit.SPISWRESET = 0;
SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;
SpiaRegs.SPICCR.bit.SPICHAR = (12-1);
SpiaRegs.SPICCR.bit.SPILBK = 0;
// Enable master (0 == slave, 1 == master)
// Enable transmission (Talk)
// Clock phase (0 == normal, 1 == delayed)
// SPI interrupts are enabled
SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;
SpiaRegs.SPICTL.bit.TALK = 1;
SpiaRegs.SPICTL.bit.CLK_PHASE = 0;
SpiaRegs.SPICTL.bit.SPIINTENA = 1;
// Set the baud rate
SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = SPI_BRR;
// Set FREE bit
// Halting on a breakpoint will not halt the SPI
SpiaRegs.SPIPRI.bit.FREE = 1;
// Release the SPI from reset
SpiaRegs.SPICCR.bit.SPISWRESET = 1;
PieCtrlRegs.PIEIER6.bit.INTx2 = 1; // Enable PIE Group 6, INT 2
IER=M_INT6; // Enable CPU INT6
PieVectTable.SPIA_TX_INT = &spiAint;
EDIS;
}
__interrupt void spiAint(void)
{
DELAY_US(1000);
GpioDataRegs.GPACLEAR.bit.GPIO19 = 1;
SpiaRegs.SPITXBUF=3244;
SpiaRegs.SPIFFTX.bit.TXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=M_INT6; // Issue PIE ACK
GpioDataRegs.GPASET.bit.GPIO19 = 1;
}