Part Number: TMS320F28377D
Hi,
I have posted before asking question about settings for EMIF related registers to talk with external SRAM. Thanks to Singh's help, I identified D12 had problem. After checking the hardware connection, I spotted that D12(GPIO72) is also connected to external switch for boot mode. I wonder if this is a problem, and how does this affect EMIF since D12 seems always to be "0" and how to solve this? Can anyone give some hints? The previous post may have beem closed because I did get feedback, so I post this new one.
Thanks,
Yi