This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: TMS320F28035 Concatenated Firmware Images

Part Number: TMS320F28035


Customer is loading firmware on multiple TMS320F28035 boards via SPI and SCI.  They need to know how to create multiple Motorola S-record hex files in CCS 6.1.3.  They aren't sure what kind of Image File to produce; a Host image or Load image.

The customer would like to create a concatenated firmware image that includes all device in the system hosted on a PC.  The PC would send images to an embedded host that would send out images to individual devices.

Customer has successfully created Motorola S-Record hex file(s), but they seem too small.  The .OUT file is 247K in size; the .HEX files are only 10K in size.

Please advise on how to configure the Load Image Options in Project->Properties->Build->C2000 Hex Utility->Load Image Options

Any advice you could offer would be appreciated.

Regards,
Mark