Part Number: F28M35H52C
Other Parts Discussed in Thread: CONTROLSUITE
Hey all,
My application requires using concerto controller and activate ARM cortex M3's Ethernet communication at 10Mbps speed, and also possibly use a Modbus TCP/IP application layer over ethernet.
So to understand the ethernet firmware implementation and a TCP application layer i was going through a example from control suite which implements iwip open tcp/ip stack on Ethernet. But it was very hard for me to follow through this example or even debug it as there is not much explanation provided as to how we can configure the hardware or how should we get going with debugging the example using CCS.
Can anyone help me understand this particular example available on control suite for concerto family of controllers. The path to the project is as follows.
C:\ti\controlSUITE\device_support\f28m35x\v208\F28M35x_examples_Master\enet_lwip
Any help or clue is much appreciated.
Thanks