This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28377S: LauchXL-F28377S Jitter on XClockout or ePWM

Part Number: LAUNCHXL-F28377S

Hi,

I would like to know if there is some information about the jitter of the SYSCLK, XClockout and the ePWM Modules and available.

I use the ePWM Module to generate a 2MHz PWM Signal (puslwidth is 25ns) for an external ADC. I am a bit concerned about the jitter quality since I can't find any specs.

Kind Regards,

Hanno

  • Hi Hanno,

    The jitter on SYSCLK, XCLKOUT, and ePWMs will largely come from jitter on the F28377S's clock source.

    Are you using one of the internal oscillator to clock the device? Or are you using an external crystal/oscillator?

    Note that the precision of the internal oscillator is provided in the datasheet.


    Thank you,
    Brett