Hi yanming and all,
We are using Lab5a with the resolver feedback. Electrical angle calculation is based on TI resolver to digital converter kit hardware and firmware.
We run the motor at 227Vrms(line to line) and 531Arms(phase). At that time motor torque was 289Nm(shaft output) and 3040rpm. But according to the datasheet of the motor, there should be 377Nm, 3863rpm at that time by considering torque constant and the backemf constant. We have a loss of nearly 50kW.
But we cannot increase rpm or line voltage further (Seems we have hit the base rpm according to battery voltage 305Vdc at that time).
We have tested data from the motor manufacture. They have run the motor with 355Nm,4000rms output at 235Vrms(line to line) and 500Arms(phase).
Point A(blue) - Current operating Point (227Vrm,531Arm)
Point C (red) - Operating point of point A, 227Vrm,531Arm according to motor datasheet. ( calculated using motor constants ke and kt)
Point B (blue) - tested data from motor manufacture for 235Vrms, 500Arms
What will be the reason for this mismatch?
Thank you