Part Number: TMS320F28335
The customer did the experiment to test signal inteference for the MCU in lab, when they inject 3.3 Volt pulse on the SCI pin of 28335 directly, all the application ISR are disable and only the main function can run. It may induce over-current on the pin of SCI, but it did not destroy the pin, and they want to know why injecting voltage pulse will affect the interrupt, what is the principle?