This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Uniflash Issue

Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH,

Hi All, 

I had a question regarding use of Uniflash with the TMS320F28335. 

A TMS320F28335ZJZQ is used in my board. It is a new board, so after testing some code, I erased the code in the DSP with the software "UniFlash". However, I found the pin C6 (GPIO46/XA6), the GPIO port,  still output 3.3V after the erasing.

It happened to all three boards that we tried this on, could that be "not-erasing the code completely" or some other issues? 

Thanks,

Ethan