Part Number: TMS320F28335
Hi,
I need to know the default state of the ePWM outputs (all six modules) when the processor starts. In section 6.2 of the 'Systems Controls and Interrupts' guide, it is said that the internal pullups are disabled by default for the ePWM pins. Does it mean that these outputs are LOW by default or are they tri state in the default condition?
I have a custom F28335 board and the ePWM outputs are all high when the processor boots up and I have not loaded any program in the RAM. This is not consistent with the description given in the guide.