Part Number: TMS320F28377S
A few questions about adding XDS100v2 to a board:
1 - Is it better to copy the XDS100v2 section of the LAUNCHXL-F28377S Overview User's Guide - Texas Instruments or the schematic here from the wiki http://processors.wiki.ti.com/index.php/XDS100?
2 - The the CPLD content at the same wiki link above the latest?
3 - Are the isolators U5 and U7 on the LaunchPad required?
4 - If 3.3V is already available on the board is there a concern with removing the VBUS to 3.3V regulator to power the FTDI device?