Part Number: TMDSHV1PHINVKIT
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hi
I am checking this kit.
I get output wave form as square shape, not sine wave.
I have attached it.
also even I can't get 50Hz by changing from given GUI. Please help me.
check attached image.
My controller card is Concerto 28x.
Here is my Solar DC_AC_settings.h file.
#ifndef _PROJSETTINGS_H #define _PROJSETTINGS_H //********************************************************************************** // NOTE: WHEN CHANGING THIS FILE PLEASE REBUILD ALL //********************************************************************************** //================================================================================== // Incremental Build options for System check-out //================================================================================== // BUILD 1 Open loop boost check + ADC feedback // BUILD 2 Complete PFC Build #define INCR_BUILD 3 #define VoltCurrLoopExecRatio 8 #define Protect_Enable 1 #define Protect_Utiligy_Enable 1 //================================================================================== // Interrupt Framework options //================================================================================== #define EPWMn_DPL_ISR 0 // for EPWM triggered ISR set as 1 #define ADC_DPL_ISR 1 // for ADC triggered ISR set as 1 //---------------------------------------------------------------------------------- // If EPWMn_DPL__ISR = 1, then choose which module //---------------------------------------------------------------------------------- /* #define EPWM1 1 // EPWM1 provides ISR trigger #define EPWM2 0 // EPWM2 provides ISR trigger #define EPWM3 0 // EPWM3 provides ISR trigger #define EPWM4 0 // EPWM4 provides ISR trigger #define EPWM5 0 // EPWM5 provides ISR trigger #define EPWM6 0 // EPWM6 provides ISR trigger */ //================================================================================== // System Settings //---------------------------------------------------------------------------------- #define HistorySize 8 #endif //_PROJSETTINGS_H
Please help me as soon as possible.
Thank you