I am using a TMS320F2812 (will refer to as DSP from here on) to communicate with an EtherCAT Slave controller that uses ET1100 chipset.
I want to establish a 8 bit SPI communication where DSP is Master and Et1100 is slave.
My problems include
1. the SPI ENABLE LINE DOES NOT WORK AS INTENDED. I want the SPI ENABLE line to become active (low) at start of communication and then go inactive (high) AFTER 8 BITS are communicated. This also leads me to the question whether after I load the TXBUF should I wait for x micro/milli seconds before loading the next TXBUF? Does this also cause the ENABLE line to not work as intended?
The following functions are to read and write to/from the et1100.
void ESC_read(uint16_t address, void *buf, uint16_t len, void *tALevent) {
uint16_t count = 0;
unsigned int *ptr;
uint16_t adr = 0;
uint16_t i = 0;
//adr = address;
adr = (address<<3)+ESC_CMD_READ;
ptr = tALevent;
// Chip select low
EALLOW;
GpioDataRegs.GPFDAT.bit.GPIOF3 = 0; // Transmit Enable (SYNC)
//SpiaRegs.SPICTL.bit.TALK = 1;
EDIS;
SpiaRegs.SPITXBUF = adr;
while ( ! SpiaRegs.SPISTS.bit.INT_FLAG );
__byte(ptr,0) = (SpiaRegs.SPIRXBUF&0x00FF);
SpiaRegs.SPITXBUF = send_8bit(adr);
while ( ! SpiaRegs.SPISTS.bit.INT_FLAG );
__byte(ptr,1) = (SpiaRegs.SPIRXBUF&0x00FF);
count = len;
ptr = buf;
while ((count--) > 1)
{
i=0;
SpiaRegs.SPITXBUF = ESC_NEXT;
while ( ! SpiaRegs.SPISTS.bit.INT_FLAG );
__byte(ptr,i) = (SpiaRegs.SPIRXBUF&0x00FF);
i++;
}
SpiaRegs.SPITXBUF = ESC_TERM;
while ( ! SpiaRegs.SPISTS.bit.INT_FLAG );
// Chip select high
EALLOW;
// SpiaRegs.SPICTL.bit.TALK = 0;
GpioDataRegs.GPFDAT.bit.GPIOF3 = 1; // Transmit DISable (SYNC)
EDIS;
__byte(ptr,i) = (SpiaRegs.SPIRXBUF&0xFF);
}
void ESC_write(uint16_t address, void *buf, uint16_t len, void *tALevent) {
uint16_t count;
uint16_t dummy;
unsigned int *ptr;
uint16_t adr;
adr = ((address<<3)+ESC_CMD_WRITE);
ptr = tALevent;
// Chip select low
EALLOW;
GpioDataRegs.GPFDAT.bit.GPIOF3 = 0; // Transmit Enable (SYNC)
// SpiaRegs.SPICTL.bit.TALK = 1;
EDIS;
SpiaRegs.SPITXBUF = adr;
while ( ! SpiaRegs.SPISTS.bit.INT_FLAG );
__byte(ptr,0) = (SpiaRegs.SPIRXBUF&0x00FF);
SpiaRegs.SPITXBUF = send_8bit(adr);
while ( ! SpiaRegs.SPISTS.bit.INT_FLAG );
__byte(ptr,1) = (SpiaRegs.SPIRXBUF&0x00FF);
count = len;
ptr = buf;
while ((count--) > 0)
{
uint16_t i=0;
SpiaRegs.SPITXBUF = send_8bit(__byte(ptr,i));
i++;
while ( ! SpiaRegs.SPISTS.bit.INT_FLAG );
dummy = SpiaRegs.SPIRXBUF;
}
// Chip select high
EALLOW;
// SpiaRegs.SPICTL.bit.TALK = 0;
GpioDataRegs.GPFDAT.bit.GPIOF3 = 1; // Transmit DISable (SYNC)
EDIS;
}
Summarizing - My primary concern is the SPI does not work as intended.
Also attaching the SPI initialization.
static void spi_init(void)
{
EALLOW;
GpioMuxRegs.GPFMUX.all=0x000F; // Select GPIOs to be SPI pins
// Port F MUX - x000 0000 0000 1111
EDIS;
DINT;
// Initialize SPI FIFO registers
SpiaRegs.SPIFFTX.all=0xA040;
SpiaRegs.SPIFFRX.all=0x2040;
SpiaRegs.SPIFFCT.all=0x0;
SpiaRegs.SPICCR.all =0x0047; // Reset on, (clk pol=1 : Falling edge), 8-bit char bits
SpiaRegs.SPICTL.all =0x0006; // Enable master mode, normal phase,
// enable talk, and SPI int disabled.
SpiaRegs.SPIBRR =0x007F; // 150 MHz/4/(127+1)= 292.3 KHz
SpiaRegs.SPICCR.all =0x00C7; // Relinquish SPI from Reset
SpiaRegs.SPIPRI.bit.FREE = 1; // Set so breakpoints don't disturb xmission
}