Part Number: TMS320F28335
I want to set a timer to count milliseconds without interrupt.
So I configure a timer (CPU frequency = 120 Mhz)
void SysTimerInit(void)
{
Uint32 prescaler;
// Make sure timers are stopped:
CpuTimer1Regs.TCR.bit.TSS = 1;
// Initialize timer period to maximum:
CpuTimer1Regs.PRD.all = 0xFFFFFFFF;
prescaler = 120000-1; //1000us->1ms
CpuTimer1Regs.TPR.bit.TDDR = (prescaler & 0x0000FFFF);
CpuTimer1Regs.TPRH.bit.TDDRH = (prescaler >> 8);
// Initialize timer control register:
CpuTimer1Regs.TCR.bit.TRB = 1; // 1 = reload timer
CpuTimer1Regs.TCR.bit.SOFT = 1;
CpuTimer1Regs.TCR.bit.FREE = 1; // Timer Free Run
CpuTimer1Regs.TCR.bit.TIE = 0; // 0 = Disable/ 1 = Enable Timer Interrupt
CpuTimer1Regs.TCR.bit.TSS = 0; // 1 = Stop timer, 0 = Start/Restart Timer
}
And functions to handle the counter
void SysTimerSet(Uint32 *compare_val, Uint32 count_ms)
{
Uint32 timer_count_val = CpuTimer1Regs.TIM.all;
*compare_val = timer_count_val - count_ms;
}
Uint16 SysTimerElapsed(Uint32 *compare_val)
{
Uint32 timer_count_val = CpuTimer1Regs.TIM.all;
return (timer_count_val <= *compare_val);
}
And I test.
SysTimerInit();
SysTimerSet(&compare_val, 100);
while(1)
{
if(SysTimerElapsed(&compare_val))
{
SysTimerSet(&compare_val, 100);
}
}
In the debugger I should see variable compare_val decremented by 100. But I see some random numbers. Where is my mistake?