Other Parts Discussed in Thread: SYSBIOS, CONTROLSUITE, TMS320F28377D
Tool/software: TI-RTOS
Hi
team
I am trying to create a sysbios project by combining the usb_to_serial project from ti provided in the control suite.
I am not able to add the corresponding files .cmd to the mapping section
Kindly please help out for adding the file and building it to get the .out
I have attached the screen shot of the directory and the error that I am getting so that let me know what files are actually missing
--include_path="C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_headers/include" -g --define=CPU1 --define=ccs --diag_warning=225 --diag_warning=255 --display_error_number --diag_wrap=off --gen_func_subsections=on --preproc_with_compile --preproc_dependency="usb_serial_structs.pp" --cmd_file="./configPkg/compiler.opt" "../usb_serial_structs.c"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 257: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 379: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 468: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 590: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 649: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 722: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 772: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 846: error #1167: invalid attribute for "struct <unnamed>"
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usblib.h", line 876: error #1167: invalid attribute for "struct <unnamed>"
>> Compilation failure
"C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/usblib/usbcdc.h", line 904: error #1167: invalid attribute for "struct <unnamed>"
10 errors detected in the compilation of "../usb_serial_structs.c".
gmake: *** [usb_serial_structs.obj] Error 1
'Building file: ../ustdlib.c'
'Invoking: C2000 Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/include" --include_path="C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common" --include_path="C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_common/include" --include_path="C:/ti/controlSUITE/device_support/F2837xD/v130/F2837xD_headers/include" -g --define=CPU1 --define=ccs --diag_warning=225 --diag_warning=255 --display_error_number --diag_wrap=off --gen_func_subsections=on --preproc_with_compile --preproc_dependency="ustdlib.pp" --cmd_file="./configPkg/compiler.opt" "../ustdlib.c"
"../ustdlib.c", line 1380 (col. 20): remark #2614-D: Use --fp_mode=relaxed to enable TMU hardware support for FP division.
'Finished building: ../ustdlib.c'
' '
gmake: Target `all' not remade because of errors.
Thank you
Deepak R