Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
Hello,
I have read through these forums as well as the user guide on interrupts (sprugl8c.pdf) extensively but am unable to find a solution to trigger a stable periodic ISR in Lab11d. There is a lot of information for control suite but no concrete examples for MOTORWARE other than timer.c as mentioned below.
What I am trying to do is trigger a lower priority ISR at around 10 milliseconds which does not interfere with the execution of motor1_ISR and motor2_ISR of Lab11d. I tried to use the included timer0ISR to accomplish this but this 5ms period seems to cause timing issues with the other 2 ISRs - I think that this is because it is linked to the TINT0 interrupt which is of higher priority than the ADC1 and ADC2 interrupts used to trigger motor1_ISR and motor2_ISR by default.
What I would like to know is - can you tell me if and how it would be possible to change the priority of TINT0 to below ADC1 and ADC2 - or alternatively replace TINTO with ADC3 (I tried this but was unable to succesfully trigger an ADC3 interrupt by modifying hal_2mtr.c) which I understand should be of lower priority than ADC1 and ADC2 by default. Is my assumption correct that this would fix the timing issues? Could you direct me to a concrete example for doing this in motorware?
Thanks in advance!
Steven