Part Number: TMS320F28375S
Hello.
I am using EMIF2 connected SDRAM, The frequency of SYSCLK is set to 200MHz.
I have two questions.
1.Are there any methods for setting the frequency of EMIF2 CLK other than the following two setting items??
・SYSCLK/1 = 200MHz
・SYSCLK/2 = 100MHz
2.If I want to set the frequency of EMIF2 CLK 133MHz, is there no way other than setting the frequency of SYSCLK to 133MHz ?
Could you give me something advises?
Regards,
uchida-k