This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

possible bug in SolarLib application library



Hi all
it seems to me that there is a bug in the proposed initialization for the function "SINEANALYZER_DIFF_F", comprised in "SolarLib" application library.
Because the initialization function "SINEANALYZER_DIFF_F_init" simply clears to zero internal fields and the description of the library suggest to initialize only the fields "SampleFreq" and "Threshold",
the fields "nsamplesMin" and "nsamplesMax" remains = 0, while they are used in the processing function to validate the detected zero-cross point.
I think they should be initialized, after the call to "SINEANALYZER_DIFF_F_init" and before the use of the computation function, to something like:

nsamplesMin = sample freq / max grid frequency
nsamplesMax = sample freq / min grid frequency

In fact, the file SolarLib.pdf suggest this initialization for the "SINEANALYZER_DIFF_wPWR_F" version of the routine (the one that calculates also the power), but these values are used also in the "lighter" version:

if(v->nsamplesMin < v->nsamples < v->nsamplesMax)
{
        // computations @zero-crossing point
}

and for this reason they need to be initialized.