Other Parts Discussed in Thread: DRV8312
I Changed the ADC Hardware mapping with my customized board based on the design of DRV8312 and F28054M
The default setting of current offsets are :
I_a connect to ADC_B3
I_b connect to ADC_B5
I_c connect to ADC_B7
I changed them to followings:
I_a connect to ADC_A1
I_b connect to ADC_B1
I_c connect to ADC_A3
I KEEP THE VOLTAGE OFFESETS MAPPING THE SAME as DRV8312
Since I changed the hardware connections, I need to change software ADC mapping as well
So I changed the ADC pin map in void HAL_setupAdcs(HAL_Handle handle) from hal.c
// configure the SOCs for drv8312kit_revD // sample the first sample twice due to errata sprz342f ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_0,ADC_SocChanNumber_A1); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_0,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_0,ADC_SocSampleDelay_7_cycles); ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_1,ADC_SocChanNumber_A1); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_1,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_1,ADC_SocSampleDelay_7_cycles); ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_2,ADC_SocChanNumber_B1); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_2,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_2,ADC_SocSampleDelay_7_cycles); ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_3,ADC_SocChanNumber_A3); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_3,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_3,ADC_SocSampleDelay_7_cycles); ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_4,ADC_SocChanNumber_B7); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_4,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_4,ADC_SocSampleDelay_7_cycles); ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_5,ADC_SocChanNumber_A7); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_5,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_5,ADC_SocSampleDelay_7_cycles); ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_6,ADC_SocChanNumber_B4); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_6,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_6,ADC_SocSampleDelay_7_cycles); ADC_setSocChanNumber(obj->adcHandle,ADC_SocNumber_7,ADC_SocChanNumber_B2); ADC_setSocTrigSrc(obj->adcHandle,ADC_SocNumber_7,ADC_SocTrigSrc_EPWM1_ADCSOCA); ADC_setSocSampleDelay(obj->adcHandle,ADC_SocNumber_7,ADC_SocSampleDelay_7_cycles); return; } // end of HAL_setupAdcs() function
After I made these changes, I am still NOT able to read correct current offsets, which supposes to get these similar values
#define I_A_offset (-0.8692960739)
#define I_B_offset (-0.8690671921)
#define I_C_offset (-0.8657041192)
BUT I am getting following values:
I_A_offset (-0.259814620)
I_B_offset (-0.247000575)
I_C_offset (-0.138281882)
Did I miss anything that also need to be changed?