This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Piccolo F28004x Development Tools and Examples

Part Number: TMS320F280049
Other Parts Discussed in Thread: UNIFLASH, CONTROLSUITE, C2000WARE, LAUNCHXL-F280049C, TMDSCNCD280049C, TMDSHSECDOCK

 

ControlCARD: http://www.ti.com/tool/TMDSCNCD280049C 

LaunchPad: http://www.ti.com/tool/launchxl-f280049C 

Code Composer Studio (CCS) and Compiler:

  • CCS Version
    • Minimum requirement: CCS v6.2.0.00050
    • Recommended: CCS v7.0.x
  • CCS - TI C2000 Device Support Package (CCSv7 Required. Check CCS for updates.)
    • Minimum requirement: v4.2.3.0
    • Contains the F28004x CCS device, gel, and register files for project setup and debugging
    • Contains the F28004x flash plug-in support (Flash API User Guide: http://www.ti.com/lit/spnu628)

  • C28x Compiler (CCSv6 - Requires Installation, CCSv7 - Included in Installation)
    • Minimum requirement: v16.9.1.LTS
    • F28004x examples setup and tested using this version.
  • Always check CCS updates for the latest version of the compiler, flash programming, and device configuration files

DSP/BIOS:

  • Will not be supported

SYS/BIOS:

  • Portions of SYS/BIOS are included in F28004x ROM
  • ROM SYS/BIOS Version: v6.42.01.10
  • Downloadable SYS/BIOS Version (With F28004x Support): v6.45.00.20

Uniflash:

Device Support and Examples:

  • ControlSUITE
    • Will not be supported
  • C2000Ware – v1.00.00.00 or newer

PinMUX Tool:

JTAG Controller Support:

  • F28004x controlCARD supports on-board XDS100v2
  • LAUNCHXL-F280049C supports XDS110 in 2-pin cJTAG configuration
  • Supported: XDS100v2, XDS200, XDS560, XDS110
  • Not Supported: XDS510USB

Codeskin 3rd Party Flash Programmer:


Tool Download Links

SYS/BIOS

Download

XDC Tools

Download

C2000Ware

Download

DigitalPower SDK

Download

PinMux Tool

Download

Uniflash

Download

  • Note that we have updated this post, including the new production version of the controlCARD: TMDCNCD280049C and the Experimenter's Kit: TMDSDOCK280049C which is offered as a virtual bundle. This just means when you order TMDSDOCK280049C our eStore sends you

    the controlCARD: TMDSCNCD280049C

    and the Experimenter's Kit baseboard: TMDSHSECDOCK.

    We are also happy to announce the low-cost LaunchPad: LAUNCHXL-F280049C

    With BoosterPack and example software support in the works!

    Also new to this post is the C2000Ware Digital Power SDK

    which includes software libraries and examples of 4 TI Designs, with new releases planned periodically.

    F28004x "S" temp devices in 64-pin and 100-pin versions are in full production and open for order entry.

    F28004x "Q" Automotive AEC Q100 64-pin and 100-pin devices will start production in September 2018.

    F28004x "S" 56-pin QFN package will be released mid 2019.